This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE11612-SEP: IBIS Model Error

Part Number: AFE11612-SEP

Tool/software:

Hello,

I'm running signal integrity sims on the AFE11612-SEP SPI and Reset pins.
The Reset uses the DAC_CLR model. The DAC_CLR_5 has Voltage Range between 1.8V - 2.2V.
I believe this is incorrect as the DAC_CLR_3 has Voltage Range between 2.7V - 3.3V.
Could someone check and verify if the DAC_CLR_5 model is correct? Thank you.