Tool/software:
Dear E2E Design Support Team and Users,
I am currently in the process of setting up pattern tests with the TSW14J57-AFE7444EVM boards, using the test files located at:
C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\Test Files
I have noticed that there is only one LTE signal with a 30 MHz bandwidth available (LTE_Freq_30MHz_Amp_0dB_BW_20.003MHz_307.2MSPS).
Given that this DAC/ADC can achieve higher sampling rates, I am inquiring whether there are additional test files available for this board, particularly LTE signal patterns with 40, 50, and 60 MHz bandwidths. Access to these files would greatly facilitate my testing process.
Thank you for your assistance.
Kind
---
Alex