This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8564: VIO=1.8V support

Part Number: DAC8564
Other Parts Discussed in Thread: DAC80504

Tool/software:

Hello,

My customer is considering to use DAC8564, but the datasheet says IOVDD=1.8V(min) which means VIO=1.8V(typ) power supply can't meet the spec to think about the variation of the external power source.  Is it your intention?  Would you please tell me the background of the spec of IOVDD=1.8V(min) that you can't support 1.7V(min)?

I see many of your products also support only 1.8V(min), so I can't suggest other devices.  If you can make it to 1.7V(min) or so, there would be many more applications since many applications these days use VIO=1.8V(typ).  It means we miss many applications.

Best Regards,

Yoshikazu Kawasaki