Other Parts Discussed in Thread: , ADC-PHI-PRU-EVM, SYSCONFIG, ADS8598H
Tool/software:
Hi,
we have a custom AM64 board where we would like to add the ADS127L18 converter. We have brought out a couple of pins from the ICSSG0 to a header which we can use, but we are not sure which pins exactly are needed to use this ADC converter with the 8 bit parallel mode.
Since we saw that there is the ADC-PHI-PRU-EVM (for am64evm) in combination with the ADS127L18EVM-PDK, this should be possible. I have checked the pins that are routed from the ADS127L18 via the adapter board to the am64, but some of the pins used are missing on our header.
I also checked the Sysconfig for the AM64 in the PRU-IO/ADC section where it shows the pin configuration for a couple ADCs (e.g. ADS8598H) with 16bit parallel interfaces, but the pins don't really overlap with the ADS127L18EVM-PDK/ADC-PHI-PRU-EVM configuration.
Now, there are a couple of questions which we have:
1. Is there a software example for the AM64 using the ADS127L18EVM, or will there be one in the future? (from that I could see how the pins are selected/configured)
2. Is it possible to change the pins freely in the ICSSG0 to fit the ADS127L18 8 bit parallel interface e.g. to our custom header?
p.s. maybe this needs to be moved to the processor/AM64 forum
Best regards,
Ergin