This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3660EVM: what is the interface and voltage on InternalDCLKIN_P

Part Number: ADC3660EVM
Other Parts Discussed in Thread: ADC3660, CDCE6214

Tool/software:

Hi team,

ADC3660 DCLKIN is from CDCE6214 OUT4_P, which is labeled InternalDCLKIN_P.

What is the output format and voltage on InternalDCLKIN_P? I'm concern because the DCLKIN abs max is 2.1V and CDCE6214's supply is 3.3V. Also PRIREF_P is DNP, so it is not biased.

REgards,

Hayashi