Tool/software:
Hello,
I was hoping you could help inform me on the best approach for filtering the supply rails given me application, as well as impedance matching advice. I don't have much experience with ADCs, let alone high bit count ADCs.
We have many cascaded stages, but below summarises what I am dealing with,
125Vrms AC input -> bucks down to +24VDC -> bucks down to +5VDC -> LDO's to 3.3VDC
The 3.3VDC is being used for AVDD as well as DVDD.
- If I want to decouple AVDD from DVDD using an LC filter (inductor not ferrite), how should I go about choosing the cutoff frequency so that I'm not exciting any resonances as well as not impeding power flow into the pin for ADS131M02
- Which frequency in the datasheet should I be designing around?
- Should I be placing the LC closer to the AVDD or DVDD pin?
- For my voltage measurement of AC line, i'm using a standard AC line voltage divider with an anti-aliasing filter near the ADC AIN pins. Should the effective resistance of the divider be equal to the differential input impedance of the pin (300k)? PGA = 1.
- For my current measurement I'm using a CT, so same relative question above but should the output impedance plus the burden resistor equal the input impedance of the AIN pin?
Cheers!