This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5474-SP: ADS5474

Part Number: ADS5474-SP
Other Parts Discussed in Thread: ADS5474

Tool/software:

I'd like to know how to use the DRY to catch the data.

Could you provide FPGA RTL codes related to the DRY?

Now I am using the RTG4 made by Microchips.

Regards

Jae-Heung Yeom

The datasheet reads:

Referencing Figure 1, the polarity of DRY with respect to the sample N data output transition is undetermined
because of the unknown startup logic level of the clock divider that generates the DRY signal (DRY is a
frequency divide-by-two of CLK). Either the rising or the falling edge of DRY will be coincident with sample N and
the polarity of DRY could invert when power is cycled off, on or when the power-down pin is cycled. Data capture
from the transition and not the polarity of DRY is recommended, but not required. If the synchronization of
multiple ADS5474 devices is required, it might be necessary to use a form of the CLKIN signal rather than DRY
to capture the data.

  • Hi Jae-heung,

    The DRY is simply the output data clock that is timed with respect to the output data. Its best to latch onto the DRY from the FPGA, then delay this DRY or output data respectively in order to satisfy timing and capturing the data.

    Unfortunately we don't have any RLT code we can share, this was done by a third party vendor that we no longer use for these types of developments.

    Regards,

    Rob