This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7038: Autonomous Mode: what happens when SEQ_START/DWC_EN are not set to 0 on alert

Part Number: ADS7038

Tool/software:

Hi,

Im trying to determine if the ads7038 is suitable for my application.

As said in the title, when in autonomous mode, will the EVENT_HIGH_FLAG, EVENT_LOW_FLAG continue to be set when entering and leaving the comparator window when SEQ_START and DWC_EN are not set to 0?

I need the high and low flags to be set and unset without MCU intervention so the can drive mosfets that bypass shunts when entering and leaving the ideal window of the shunt as fast as possible.

Or are the low and high flags only set again after clearing them.

Page 26: of the datasheet:

The idea is that the MCU will only poll the LAST_VALUE_CHx register for the value and show the value on a display and that this code should not delay the driving of the mosfet.

regards,

Klaas-Jan