Part Number: ADC3662
Other Parts Discussed in Thread: , THS4541
Tool/software:
Hi,
I'm using the ADC3662 with the THS4541 as FDA like at ADC3662EVM.
In the datasheet of the ADC3662 it's mentioned that protection diodes may be needed to protect the ADC from over-voltage. There are no such diodes at the ADC3662EVM and in chapter 8.3.1 Analog Input are diodes sketched in. So my question is, above which voltage level at xINP/M should I protect the ADC? And below which voltage level are the internal diodes sufficient?
Thanks for help!