Other Parts Discussed in Thread: TSWDC155EVM
Tool/software:
Hi,
I'm looking at the ADS9219EVM and TSWDC155EVM with the GUI (CGui_ADS92xx_EVM_GUI) and I have two questions:
(1) Is the FPGA_SMPL_SYNC generated by the GUI (FPGA)? I do not see any options in the GUI to enable/disable the SYNC? I want it enabled, could be disabled using jumper (JP4).
(2) There seems to be a problem with the display of left side Controls panel (see screen grab below),
where some of the controls are not fully visible, some sort of sizing problem (the inner box does not follow the controls panel). The GUI is installed on a Win11 machine.
Any ideas on how to fix this? Missing fonts? Change screen resolution (I'm using 3840x2160, 200%).
Thanks you,
Sven.