Tool/software:
Hello,
This is Kwonjoon Lee from South Korea.
I always appreciate TI's accurate and fast feedback.
(Questions)
1. The datasheet of DAC81404 (5/53 page) specifies that pin voltage of OUTX to GND cannot exceed AVDD+0.3V.
I would like to ask if the OUTX pin of the DAC81404 can be driven by voltage source corresponding to 5V in the case that the DAC81404 is fully turned off
(in other words, in the case that the low dropout regulators connected to AVDD, DVDD, and IOVDD of the DAC81404 are disabled).
2. Furthermore, I would like to ask if the OUTX pin of the DAC81404 whose power supplies are fully turned off can be driven by
voltage source corresponding to 5V when a maximum driving current of the voltage source is limited to 9mA (under 10mA).
Best regards,
Kwonjoon Lee