The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1131: ADCs and ADC Mux for high temperature application (above 150C)

Part Number: ADS1131
Other Parts Discussed in Thread: ADS8320-HT, ADS1278-HT, ADS1278

Tool/software:

Hi,

I am in the need of high temperature application i am in the need of ADCs and ADC Mux IC above 150C.

With 24 bit resolution or greater than 12bit.

Thanks

  • Hello Sagar,

    TI only has 2 precision ADCs rated for 150C or higher.

    ADS8320-HT:
    16b, single channel, SAR ADC, -55C to 210C

    ADS1278-HT:

    24b, 8 simultaneous channels, Delta Sigma ADC, -55C to 210C

    If using a 24b device (delta-sigma), then simultaneous sampling is usually required due to latency of the internal digital filter, which is exactly what the ADS1278-HT is used for.  Assuming you need 8 channels or less, then no multiplexer is required.  If more than 8 channels, the ADS1278 can be daisy-chained with multiple parts to extend channel count.

    ...

    I did a quick check and do not see any hi-temp MUX devices available above 150C.

    Regards,
    Keith Nicholas
    Precision ADC Applications