Part Number: ADS1258
Tool/software:
Hi
We have design based on ADS1258
We want to add external protection to ADC input for Overload\Overvoltage Protection
As the data sheet suggest in P.41 to add BAT54SWTI to ADC Input lines

BAT54SWTI Spec :


How this diode with V_Forward (~400mV) and Reverse protect ADC input ports ?
We have input signal of -4V to 4V in the ADC Input
BAT54SW Seems not let signal above and below ± 1000mV go into the ADC

Should we use 2 Zener diode with ~4.3V like BZX84C4V3S-7-F for over voltage protection ?

Data sheet : https://www.diodes.com/assets/Datasheets/ds30108.pdf
Thanks in advance