Part Number: ADC12DL3200EVM
Tool/software:

Hi,
What is the purpose of the series resistors used in reference design?
How it needs to be calculated?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12DL3200EVM
Tool/software:

Hi,
What is the purpose of the series resistors used in reference design?
How it needs to be calculated?
Thanks
Hi,
These are just to slow down the edge coming out the level translator. The R is based on the C of your line and the edge rate you want to slow it down to.
Regards,
Geoff
Hi Geoff,
In our design we plan to connect these signals directly from ADC to FPGA. In such case, are these series resistors required?
If yes, is there any calculation you can point me to choose these resistances?
We will be connecting CALSTAT, CALTRIG and PD also interfaced with FPGA directly. Are similar resistors required on those nets as well?
Hi Nandini,
No, you do not have to add series resistors. They were put in just in case we needed to adjust the output rise time by limiting the current.
Regards,
Geoff
Hi Geoff,
I plan to add a series 0-ohm placeholder just in case we encounter the need to tune the rise time.
Hope that is ok to do without any adverse effects..
Thanks
Nandini
Hi Nandini,
Adding the 0ohm resistors should not be an issue.
Regards,
Rob