Part Number: TLA2022
Tool/software:
My question is with regard to VDD verse the FSR (full scale range). The text in section 8.3.3 says that with Vdd = 3V3 and FSR set to plus/minus 4.096V, only signals up to 3V3 can be measured.
Question: how can it measure a plus/minus 2.048V signal when the supply is signal sided 3V3? Would it not only read plus/minus 1V5? or does the device generate its own negative rail that is not shown in the datasheet?
My plan is to TLA2022 for AC current measurement. I want to determine the CT burden load to maximize my resolution into the ADC. This bit of confusion on how this IC works with regard to range and rail voltages results in a half/double issue on the burden resistor values. Not hard to fix on my prototype, but better if the load is correct straight off the production line.
Thanks for your help,