Part Number: ADS8688A
Other Parts Discussed in Thread: ADS8688,
Tool/software:
When a negative voltage is input to the ADS8688, an A/D conversion value in the vicinity of “0B***h” is output.
This A/D converter can be set to various voltage ranges,
The circuit uses a range of 0V to 5.12V.
When a negative voltage is input, it is expected to stick to “0000h”, but in reality, values between “0B00h” and “0BFF” are output. The datasheet does not list negative voltage output, so please let me know the output specifications.