Part Number: AMC7836
Other Parts Discussed in Thread: LMP92066
Hardware Query Type: Reference Schematics and feasibility of Operation
Hi Experts!
We want to use the AMC7836 for GaN High Power Amplifier Biasing. Along with that, we want to integrate an external SPI-based memory into the Circuit, which allows the Bias controller (AMC7836) to automatically operate based on a pre-programmed flow of operation. Provided the memory is programmed once every power-up cycle of the system. In this regard I have some doubts and would appreciate some help:
- Is the above operation feasible with the AMC7836 device? Since AMC7836 looks like an SPI Slave device.
- Any Reference schematics for the above operation (if available), particularly the Memory integration part.
- Concerning the PA Biasing circuit, Can the Bias Controller GND be directly shorted to the RF GND in layout? (Provided the gate has a knee voltage of -5V and is biased at around -2.75 V, at a Drain voltage of 48V. The Gate Voltage is coming from the AMC7836 DAC Groups.
Any help on the above topic is highly appreciated. Thank you.