This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8365: Simultaneous sampling ADC in Smallest Form Factor

Part Number: ADS8365
Other Parts Discussed in Thread: ADS7864, ADS8363

Tool/software:

Hi TI,

In my custom board ADS8365 ADC is selected, but size is not feasible on my board.

So, Could you please suggest ADC part number which Simultaneous sampling ADC, Single ended more than 4-channel ADC.

Input Voltage Range : 0 - 5 V

Sampling rate : more than 250 KSPS

Resolution : More than 12 bit (preferred 14 or 16 bit)

Form Factor/Package : smallest (less than 6mm X 6 mm)

No of Analog inputs : 5 No of channel  , Single-Ended