This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS5651A: THS5651AIPWR Clock Frequency Range.

Part Number: THS5651A

Tool/software:

Hello,

For DAC part THS5651AIPWR, there are few clarifications required.

1. There is clock input pin "CLK", what is the frequency range for this input?

2. Referring to Figure 29. Timing Diagram in datasheet, there is clock signal. Is this the same clock signal that is provided as input from "CLK" pin?

3.The time period for clock signal in Figure 29. is mentioned as "1/fCLK". And fCLK range is given 70MSPS(min.) and 100MSPS(typ.) at 3.3V operation. For example, if fCLK is considered 100MSPS, what will be the  frequency value of "fCLK" in Hertz(Hz)? Please explain