This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5851: Analog Input channels influence each other with DC coupling inputs

Part Number: AFE5851

Tool/software:

1. Testing for the AFE output setup

  • All the signal VOUT_S<0>, …, VOUT_S<15>, VOUT_S<16>,…,VOUT_S<31> are tied together, and could be adjusted by a on board pot
  • The another signal ( DAC-OUT0,…, DAC-OUT31 ) is controlled by separate DAC, which could be output 0 – 1.4V with 10 bits resolution
  • AFE input: AFE-AIN0 = DAC-OUT0 + VOUT-S<0> / 2
  • CLAMP-H2 = 1.17V, and CLAMP-L2 = 0.375V. They are used to protect the AFE inputs for out of range signals

2. Problems Observed for CH to CH influence

  • If we set all the VOUT-S<> to 1V, and DAC-OUT<> to 0.95. All the channels are sampled to a value closed to -300 with certain gain.
  • Then we change DAC-OUT0 to 0.7V, and the CH0 reading is closed to -1600; However other channels in AFE1 readings are jumped to around -700, and all the channels in AFE2 reading are still around -300. They are using the same external reference 1.4V.
  • Do you see anything wrong with this? Or we overlooked something  in the register settings?