This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC101C021: Pull-up resistor voltage

Part Number: ADC101C021

Tool/software:

Hi, Staff
When the VA of the ADC101C021 is 3.3V, is it possible to use the Alert pin with the pull-up resistor voltage pulled up to 5V?

In this case, is it okay to set the pull-up resistance value so that it does not exceed the current limit of 15 mA?

best regards
cafain