Other Parts Discussed in Thread: DAC7564, DAC63204, DAC60504
Tool/software:
Hello TI,
Currently I am working on a project that includes an Analog section that requires an Digital to Analog Converter to be interfaced with a microcontroller through SPI communication on 3.3V levels, while Output signals are based on 5V levels. So, after searching for the DAC IC, I thought that DAC7554 could be best option. But, while reading the Datasheet I noticed that VREF cannot be greater than VDD. In my case, VDD = 3.3V and VREF or VIO = 5V
As an alternate, DAC7564 seems more promising, as it is mentioned in Datasheet that AVdd and IOVdd are separate supply rails. Am I on the right track for selection of DAC IC as per my requirements mentioned above? Or can you suggest any better alternative that perfectly suits my project requirements ?
Awaiting your response.
Thanks,
Priyanshu