Other Parts Discussed in Thread: AMC131M03EVM
Tool/software:
I am using an AMC130M02 for an isolated power bus voltage and current measurement, but have so far had no luck in establishing solid communication with the device to configure it. At one point we thought we had it configured and the DCDC was definitely running, but our board (custom based on datasheet example) will not enable the DCDC now and more interestingly, there appears to be no voltage at the DCDC_CAP output, which I did not think depended on configuration.
Should there always be a voltage (we measured ~2.6V) on the DCDC_CAP pin regardless of configuration state?
With the DRDY~ pin tied high with a 100kohm resistor (as was done in the datasheet example and on the AMC131M03EVM) how should we determine when the device is ready for communication after a POR or reset?
I did not notice in the datasheet any required long wait periods for communicating after POR or reset, but the AMC131M03EVM waits 1s between each communication after reset, taking 4s until the DRDY~ pulses start. Do we also have to wait ~1s after any kind of reset to establish communication with the AMC130M02?