Tool/software:
Hello,
This is Kwonjoon Lee from South Korea.
I would like to ask about the absolute maximum ratings of TLV5624.
(Detailed Questions)
1. What is a voltage range of OUT pin? (in terms of the absolute maximum ratings)
2. Is there an internal clamp diode between VDD and OUT?
3. In the case that there is an internal clamp diode between VDD and OUT,
What is a maximum allowable current through the clamp diode?
What is a maximum allowable current of OUT pin?
4. In the case that VDD = 0V, and there is a current flowing into OUT pin
(through a resistor between OUT and an another low-impedance node),
What is a maximum allowable current of OUT pin?
Best regards,
Kwonjoon Lee