Part Number: ADS1231
Tool/software:
hi sir
we would like to cost down the AD7780,
Did the ADS1231 is the best solution to replace ADI/AD7780?
If yes, did you have compare table?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1231
Tool/software:
hi sir
we would like to cost down the AD7780,
Did the ADS1231 is the best solution to replace ADI/AD7780?
If yes, did you have compare table?
Thanks
Hello Alex,
The ADS1231 is the best alterative device to the AD7780. Please find the comparison of the two devices below.
|
Competitor |
TI |
|
|
Parameter |
AD7780 |
ADS1231 |
|
Description |
24-Bit Pin-Programmable Low Power Σ−Δ ADC |
24-Bit, 80SPS, 1-Ch Delta-Sigma ADC for Resistive Bridge Sensors & Weigh Scales |
|
Resolution (Bits) |
24 |
24 |
|
Sample rate (max) (ksps) |
0.0167 |
0.08 |
|
Number of input channels |
1 |
1 |
|
Interface type |
SPI |
SPI |
|
Architecture |
Delta-Sigma |
Delta-Sigma |
|
Input type |
Differential |
Differential/Single-ended |
|
INL (ppm of FSR) |
±6 |
±8 |
|
Offset Error (μV) |
±10 |
10 |
|
Gain Drift (ppm/°C) |
±2 |
±2 |
|
Multichannel configuration |
Integrated PGA |
N/A |
|
Rating |
Catalog |
Catalog |
|
Reference mode |
External |
External |
|
Features |
ADC Integrated PGA |
50/60 Hz Rejection/Oscillator/PGA |
|
Operating temperature range (°C) |
-40 ~ 105 |
-40 to 85 |
|
Price|Quantity (USD) |
4.79 |
1.997 |
|
Package type |
14-Lead SOIC 16-Lead TSSOP |
SOIC |
|
Pin count |
16 |
16 |
|
Package area (mm^2) |
32.6 |
59.4 |
|
Package size (L x W) (mm) |
5.1 x 6.4 |
9.9 x 6 |
|
Power consumption (typ) (mW) |
115.0 |
5.0 |
Regards,
Jiyah Starks