This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7138-Q1: Regarding unused port

Part Number: ADS7138-Q1


Tool/software:

Hello experts,

ADS7138-Q1 has 8 channels.

We will use 5 or 6 channels in it.

Is it possible to connect a pull down resistor (about 100k ohm) to unused ports to avoid unpredictable behavior?

Best Regards,

Toru Kimura.

  • Hi Kimura-san,

    It is best that unused channels be grounded directly with a trace to avoid any noise from being introduced to the analog inputs by leaving them floating. Is there a particular justification to use such a high value, weak pull-down resistor? I would think if a pulldown were to be used, it would be a lower value, strong pull-down resistor. 

    Regards,
    Joel

  • Hi Joel-san,

    Thank you for your answer.

    >Is there a particular justification to use such a high value, weak pull-down resistor?

    There is no reason to use high value resistor.

    We want to connect to GND if is it possible.

    Is it possible to connect GND?

    And in this case, should the unused ports that connect to GND be configurated as analog inputs?

    Best Regards,

    Toru Kimura

  • Hi Kimura-san,

    Yes, the pins can be configured as analog inputs, which they are by default. They can be connected directly to ground.

    Regards,
    Joel

  • Hi Joel-san,

    Thank you for your reply.

    I understood it.

    Best Regards,

    Toru Kimura