Part Number: DAC38RF84
Tool/software:
Hello,
I am driving the DAC38RF84 from an FPGA and do not require synchronisation of the DAC with any other devices.
I gather from reading other posts that the SYSREF input signal is required regardless for subclass 1 and the internal SYSREF generator (LCMGEN) should not be used. As such I have a few questions about the use of SYSCLK:
The recommended start-up sequence in the datasheet says "Start SYSREF Generation" following the VCO tuning process. Does this mean enable the external SYSGEN source (rather than set some register field)?
Can I simply use the same external DACCLK source frequency (250 MHz in my case) as the SYSREF source?
Does the external SYSRF source need to be disabled during start up until after the VCO tuning or can it run continuously?
If it has to be started only after VCO tuning, can I disable SYSREF after the startup sequence is completed, or is it best to keep this signal operating during normal operation?
Thanks