Other Parts Discussed in Thread: REF6225,
Tool/software:
Dear Experts,
The design circuit diagram is as follows. During debugging, we found that the sampled voltage value will experience a jump, which is the actual voltage value or half of the actual value. The reference benchmark is 2.5V, and the chip used is REF6225. The value written in CONFIG1 is 0X3B, CONFIG2 is 0X08, CONFIG3 is 0x16, and CONFIG4 is 0X80. The input voltage has been set to 2 * REF, but the sampled data still jumps. We are currently unsure of the cause and hope you can help us find the reason. Thank you very much
Design schematic diagram:
Configure registers: