Tool/software:
I'm using the ADS1234 to measure a bridge.
The reference voltage is 2.5V. If I use a GAIN of 64, what will be the maximum voltage that the ADC can read?
Is the calculation 0.5Vref/64?
Second question: Since the component operates in a two's complement configuration, will the maximum readable voltage be Vref/2?
Is there a way to bypass the two's complement format?