Other Parts Discussed in Thread: ADC09SJ1300
Tool/software:
Hello, experts.
When I tried the operation of subclass 0 under the following conditions, I encountered a problem where I could not see ADC data. Perhaps TI-JESD204C-IP is not generating LMFC.
- ADC: ADC09SJ1300 ⇒ Subclass 0 (not using SYSREF)
- TI-JESD204C-IP: Release-v1.10-LATEST ⇒ Subclass 0 (not using SYSREF)
- fs=1250Msps, JMODE11(4 lanes, 9 bit, 8B/10B), flinerate = 5Gbps (= 4 x 1250 M)
Please tell me two things.
- If ADC09SJ1300 and TI-JESD204C-IP are both subclass 0 (not using SYSREF), is flinerate=5Gbps operational? Is this case supported? Or do you need to keep flinerate ≦ 3.125 Gbps?
- In addition, LETTER IDENTIFIER=h in Table 8-9 of ADC datasheet states: "Not supported, but subclass1 transmitter is compatible with subclass0 receiver."
What kind of case does this show? Does it mean that the combination of ADC= subclass 1 (using SYSREF) and IP= subclass 0 (not using SYSREF) is acceptable?