Other Parts Discussed in Thread: AFE53902-Q1, AFE539F1-Q1
Tool/software:
Can AFE53902-Q1 be used for a constant power dissipation application similar to AFE539F1-Q1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE53902-Q1, AFE539F1-Q1
Tool/software:
Can AFE53902-Q1 be used for a constant power dissipation application similar to AFE539F1-Q1?
Hi Marie,
AFE539F1 has a preprogrammed transfer function that relates the ADC input voltage to a PWM output.
AFE53902 is similar in that it translates an ADC input voltage to a related output voltage or PWM out, but instead it allows the user to program up to three output slopes rather than using the preprogramed transfer function in the AFE539F1. I suppose it is possible that you can program these slopes in a profile that would allow you to achieve constant power dissipation.
Why would you not want to use the AFE539F1?
Best,
Katlynne Jones