This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1115-Q1: Question about the on resistance Ron of the MUX at the input of the ADC

Part Number: ADS1115-Q1
Other Parts Discussed in Thread: ADS1114-Q1,

Tool/software:

Hello,

I am looking to get an ADC for a project I am working on.

At first, I thought of getting the ADS1114-Q1, but because I have multiple inputs, I might go with the ADS115-Q1 which can accept 4 inputs with a MUX.

The problem I am facing is that I want a precise reading between channels and if the On-Resistance Match Between Two Channels (ΔRON) is too high, my reading will change depending on which input I choose.

I would like to know if there is a way to know or calculate On-Resistance Match Between Two Channels (ΔRON) for the ADS1115-Q1.