Part Number: ADC3663
Other Parts Discussed in Thread: SN65LVDS100
Tool/software:
Hi Team,
Customer are testing with our ADC3663 connecting with Xilinx 7035.
They are considering the different voltage standard between ADC3663 datasheet and FPGA datasheet about SLVDS and LVDS
I have see some E2E question regarding the signal standard, but I am not sure if we need a translator or we can directly connect ADC3663 and FPGA.

- DCLKIN usage
FPGA can output a signal with 1 to 1.425V VCM which typical value is 1.2V and 247 to 600mV which typical value is 350mV VOD to ADC3663
ADC3663 input specification is 1-1.3V with 1.2V typical value and 200 to 650 mVpp VOD with typical value 350mVpp
- Data Lane
ADC3663 can output 1.0VCM with 500 to 850mVpp VOD.
FPGA can receive 0.3-1.425V with typical value 1.2V and 100mV to 600mV VOD
My question is:
How to understand the input VCM and VOD in ADC3663, Is that means we can accept any VCM voltage between 1 and 1.3V and VOD between 200 to 650mV, How ADC3663 recognize High and low signal?
Could ADC3663 directly connect with FPGA? Or we need some AC coupling+Bias method or translator?
Thank you,
Yishan Chen