Other Parts Discussed in Thread: LMX1204, DAC39RF10
Tool/software:
Hello,
I am looking to control the LMX1204 component on the DAC39RF10EVM evaluation board in order to configure it as follows:
- LMX CLKp: 1.28 GHz (SMA100B)
- Multiplier mode x4
- CLKout3 enable to observe a 5.12 GHz output signal on the J9 (CLK3p) connector.
However, when I attempt to modify the associated registers (Register 25, address 0x19, bits 5:3 and 2:0) in the DAC39RF10 GUI software, it does not work. Register 25 is not editable and remains at a value of 0x0103, unlike the other registers, which I can write and modify.
Thank you in advance for your response.
Best regards,
Lucas Genet.
Thales LAS FRANCE SAS - Ymare