Other Parts Discussed in Thread: DAC82002
Tool/software:
Hi TI,
I have 2 questions that I hope you can help with.
1. The Datasheet for DAC82001 (and DAC82002) lists the noise to be 10nV/sqrt(Hz) at 10kHz, but figure 6-21 shows the noise to be ~30nV/sqrt(Hz). In another thread (https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1361750/dac82001-output-noise-0-1---10hz-graph) the figure is mentioned as being inaccurate of DAC82001's true noise performance. My question is if the figure is correct in the 1kHz to 1MHz range or if there is another figure to use?
2. Figure 6-23 shows the clock feedthrough. Is this for both outputs (DAC82002) or does the channels differ in digital feedthrough?
Best regards.