Tool/software:
Hi,
I am using an ADS1261 designing a force plate with four loadcells, my object is sampling the sensor at 1000hz, according to ads1261's datasheet tab8 and sbaa535a, when I use below parameters,
filter type: SINC5, datarate:40000, chopping: disabled, # of channels :4, the calculated system cycle time is: (0.179+2*(1/40)) *4 = 0.916ms.
I want to confirm the result, or if there is some wrong calculation, the 1000hz is easy to process for the data analysis.
Thanks very much