Tool/software:
Hi team,
If an OPAMP is connected to the OUT0/1 and operated, the output will short after few hours of operation.
However, there is no similarity in the time of shortage.
Could you tell me about possible causes of shortage?
BR,
Kengo.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
If an OPAMP is connected to the OUT0/1 and operated, the output will short after few hours of operation.
However, there is no similarity in the time of shortage.
Could you tell me about possible causes of shortage?
BR,
Kengo.
Kengo-san,
I'm not sure I understand this question. Can you provide a diagram of how the opamp would be connected? Is the opamp connected as a buffer or is it trying to drive an output.
In voltage output mode, the DAC63202 output can drive a 50mA to 60mA at the output in short circuit. This is a large amount of current and that in itself can cause problems for other devices if the current is routed into them.
Regardless, a circuit diagram would certainly help to understand what could be happening.
Joseph Wu
Hi Kengo-san,
This is unusual behavior. What are the supplies of the external op amp and what DAC output have you configured?
What is actually shorting in the circuit? And how are you determining that this is a short?
Best,
Katlynne Jones
Hi Katlynne-san,
Thank you for your reply.
Bellow is registers as setting.
Register | Default | After | |
1 | COMMON_TRIGGER | 0x0000 | 0x5A00 |
2 | COMMON_CONFIG | 0x0FFF | 0x1E03 |
3 | DAC_0_VOUT_CMP_CONFIG | 0x0000 | 0x1400 |
4 | COMMON_CONFIG | 0x0FFF | 0x1003 |
5 | DAC_1_VOUT_CMP_CONFIG | 0x0000 | 0x1400 |
6 | COMMON_CONFIG | 0x1003 | 0x1001 |
I measured the resistance on the device itself.
*The value was the same in the mounting condition.
BR,
Kengo.
Hi Kengo-san,
It looks like you are enabling current mode and voltage mode for channel 0. You should write 0x1201 to enable the internal reference and power on channels 0 and 1 in voltage output mode.
Best,
Katlynne Jones