Hello Forum,
I'm hoping that someone else has worked with this combination of boards and can offer some advice. I've installed the software (TSW1200_v2p5) and connected the boards with power for the ADS5400EVM coming from the TSW1200 banana jacks. I connect a sine wave generator with varying frequency and amplitude signals to the J1 (AIN) connector on the ADS5400EVM. I select the ADS5400 as the ADC, Set the ADC Sampling Rate and Record Length and Capture a Time Domain signal. But what is displayed seems only slightly correlated with the signal that I supply. For example, the attached screen shot shows 4096 samples collected at 400Msps of a 50MHz 1 Vpp Sin wave.
Any ideas or suggestions? I have 2 sets of boards and they both behave similarly so whatever I am doing wrong is at least consistent.
Thanks for any help.
Larry Byars