Other Parts Discussed in Thread: DAC81402,
Tool/software:
Hello,
The data sheet for the DACx1401 suggests that the VSENSEN input should be connected to ground but does not explain whether this required. Is it possible to lift VSENSEN from ground so that a low-side current sense resistor can be inserted between VSENSEN and ground? In that case does the device still control VOUT correctly, that's to say maintaining exactly the requested voltage between VSENSEP and VSENSEN, provided VSENSEN is kept well below its absolute maximum of +0.3V (e.g. limited to a maximum of +0.1V)?
While I'm asking: am I right to assume that a high-side current sense resistor can be inserted between VOUT and VSENSEP without any problems, assuming there is enough voltage headroom for the DAC to compensate for it?
I noticed that on the DAC81401EVM, both VSENSEP and VSENSEN are brought out to jumpers which allow them to be disconnected from VOUT and GND respectively, so I am guessing that the DAC will correct its output for small (current sense) voltages in either the high or low side are both supported.
Are there any disadvantages, specifically for the DAC1x401, of using low- vs high-side current sensing?
Thanks,
Ian