Part Number: DAC8565
Tool/software:
Hi TI expert
Could DAC8565 output 3 signals of 100kHz at the same time, the signal is one of sine wave, square wave and triangle wave?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I can't see the image you attached.
The max SPI frequency is 50MHz, and each DAC update takes 24 SPI clocks. This is about 2.08MSPS.
With that you could achieve a 12-point sine wave, 12-point triangle wave, and 2-point square wave at ~80kHz. You could achieve a 9-point sine wave, 9-point triangle wave, and 2-point square wave at ~104kHz.
Best,
Katlynne Jones