This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1336: isolated 4-20mA receiver

Part Number: AMC1336
Other Parts Discussed in Thread: AMC1305M25

Tool/software:

is the AMC1336 a good choice for an isolated 4-20mA receiver? 

  • Hi Hanno,

    Could I know more about the application and who is the customer? 

    The AMC1336 could work for an isolated 4-20mA receiver, but depending on requirements other devices could be considered as well. The AMC1336 is an isolated modulator so it has digital output. Is there a requirement for digital output over analog? What type of interface does their microcontroller offer? Was the customer previously using the AMC1305M25 from the original question linked?

    Another consideration may be the AMC1351. This is an isolated voltage sensing amplifier with a 0-5V input range. It will have an analog output, so would need an ADC to translate the output to a digital signal again. Typically, for 4-20mA receivers we've seen that translated to 1-5V which is why this device's input range may be suitable. 

    Please let me know if you could provide any more background so I can further help or if there are any questions. 

    Best regards,

    Eva