Part Number: DAC81408
Tool/software:
Hi team,
Upon checking datasheet 9.3.1.1, it seems that the output voltage range for each channel can be determined by the register.
When switching the output voltage range for each channel (for example, outputting -10 to 10V, -5 to 5V, and 0 to 40V for different channels), will the voltage conversion accuracy be unaffected even if the power supply voltage is not switched?
In this case, should I input a power supply voltage of -10V to 40V to cover all output voltage ranges and consider the headroom value?
Best regards,
Kyohei