Part Number: ADS7835
Tool/software:
Dears:
DS mention that VREF pin need connect a 2.2µF tantalum capacitor , Could you please help check why it has such requirement ? if customer use 2.2uF ceramic capacitor , any risk here ? Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS7835
Tool/software:
Dears:
DS mention that VREF pin need connect a 2.2µF tantalum capacitor , Could you please help check why it has such requirement ? if customer use 2.2uF ceramic capacitor , any risk here ? Thanks.

For ADS7835, tying a 0.1µF ceramic capacitor to VREF at pin 1 is typical for stability, especially when using internal reference. External VREF needs careful layout to avoid noise coupling. If you're sourcing precision capacitors or compatible analog components, Jotrin has a great selection of ADC-related parts that can simplify prototyping and ensure compatibility with TI's data converters.
Hi Ben,
No worries - welcome to our e2e forum! Short answer is that yes, you can use a ceramic cap. Longer answer would involve you reading up on the differences between the two which you can do here: https://www.kyocera-avx.com/docs/techinfo/CeramicCapacitors/mlc-tant.pdf Since the 2.2uF is on the reference, using a good quality cap (X7R type) will help to maintain stability which is important for overall conversion accuracy.
Tom:
based on datasheet, 2.2uF is recommend to use tantalum cap which ESR is more larger than ceramic cap, I think that can cause stability issue. Please help confirm it .Thanks.
You can add a series resistor to compensate for the ESR of the tantalum cap.
Tom:
As datasheet don't mention when use internal reference need to add extra resistor to keep system stable. Please help confirm this .Thanks.
Haiwen,
Ceramic capacitors were not as common as they are today when the ADS7835 was released (25 years ago). I suggest that you find a capacitor footprint option that could accomodate either a ceramic or tantalum capacitor and try it out.