Tool/software:
Hi,
Is the range for AVDD 4.75V to 5.25V as specified in the pinout descriptions or would a 3.3V rail be acceptable? There is no recommended operating condition for the voltage outside of the 4.75V to 5.25V, so I wanted to confirm that that was indeed the recommended operating condition for AVDD. Abs max is –0.3V to 6V, but it is unclear if 3.3V is outside the recommended condition but within abs max ratings.
Thanks,
Lauren