This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7142-Q1: Design support for the ADC

Part Number: ADS7142-Q1


Tool/software:

Dear Team TI, I was looking forward to implement ADS7142QDQCRQ1 ADC in my design and I was going through application note of it. I could see in the formula that "100 kΩ at 25°C with a B(25/85) value of 3977" is considered. Can I consider a B(25/100) for calculation in the formula as in the NTC data sheet which I'm using, I can see B(25/100) only? Thank you, Best Regards, Srujan L