This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63204: Regarding Voltage Margin DAC

Part Number: DAC63204
Other Parts Discussed in Thread: DAC80504,

Tool/software:

Hi Team,

Please Suggest a Part Number for voltage margining DAC with high resolution 16bit with both Voltage and Current output.

Also the part should be programmable either via I2C or SPI.

Please kindly suggest a part number.

Regards,

Bhuvaneshwari K

  • Hi Bhuvaneshwari,

    Why is both current and voltage a requirement? You would not need to use both at the same time. DAC63204 is the only device that has both the current and voltage output in one device. You could consider DAC80504 for a 16-bit voltage output DAC. 

    Best,

    Katlynne Jones