This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7138: AVDD supply for ADS7138 and INA2191A1 using 4.096 reference

Part Number: ADS7138
Other Parts Discussed in Thread: INA2191

Tool/software:

Hi,

i am using (LT1790 max 5mA) for 4.096 reference of ADS7138. Since i also had INA2191 suitable for this line, i have added it on 4.096 reference.

I am little concerned if ADS7138 and INA2191A1 combined can load LT1790 eventhough datasheet electrical data says less than 1mA together.

Do you think the attached circuit is fine?

for digital lines i have used 3v3 supply as both AVDD and DVDD are independent.