Other Parts Discussed in Thread: DAC5672, DAC81404
Tool/software:
Hi,
I searched for a high-speed DAC by sorting as shown in the following URL, but I could not find any product that can use unipolar output and bipolar output separately.
1. Is it correct to understand that DAC5687 and DAC5672 only use unipolar output?
2. Also, could you introduce products that satisfy the following conditions?
・Parallel interface
・Sampling rate: 125 MHz or higher
・Resolution: 14bit and 16bit
・Number of channels: 2~4
・Output: A device that can be used between unipolar and bipolar.
Best Regards,
Nishie