This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS52J65: AD converter ADS52J65 URGENT help request. No Analog data or ADC TEST signals after PHY

Part Number: ADS52J65


Tool/software:

AD converter ADS52J65 URGENT help request. No Analog data/TEST signals after PHY

Working on our own custom PCB with XILINX UltraScale+ FPGA connected to ADS52J65 chip we stuck dfinitelly with trying to receive any data after FPGA PHY sederialisation IP.

What we achieved so far:

1. ADC is powered OK with all the necessary voltages (1,15V and 1,8V)

2. ADC is properly reset and fed with register setting values.

3. Deserialisation IP in FPGA receives proper JESD204 "CGS" phase K28.5 symbols (after 10b/8b decoding certainly)

4. JESD204 "ILAS" phase passed succesfuly with all the R, A, Q and C link configuration bytes.

5. JESD204 SYNC signal is HIGH and stable.

but after end of ILAS phase FPGA PHY data output is constantly ZERO, no matter we set default ADC data from analog

S/H part or set any ADC test pattern (ramp, all '1', 0xAA 0x55 toggle etc.). Demodulator part is disabled forcing direct

ADC/TEST data forwarding to ADC's JESD serialisation part according to datascheet. On FPGA PHY output we see

Link layer test patterns e.g. repeated transmission of a lane alignment sequence.

When we clear TRANSPORT_LAYER_TESTMODE_EN bit, after CGS and ILAS phase we should see either raw samples of

analog data or choosen ADC Test Pattern depending on EST_PAT_MODES register setting but we get ZEROs after comlete

ILAS phase. FPGA JESD204 IP (following PHY IP) shows all status and synchronization signals OK.

Help us overcome this strange behaviour please! Do we missed so crucial setup or register setting?

Thaank you in advane for all your cystomer support and Waiting for QUICK rely.

Best Regards

Wojciech Lesniak