This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC11001A: DAC81001, DAC91001, DAC11001: How long does temperature calibration take?

Part Number: DAC11001A


Tool/software:

I find no reference for the duration of the DAC internal temperature calibration cycle.

The data sheet says I can poll a status bit via SPI, or use the ALARM pin to find out when it is done.

Both of these are inconvenient in my design.

I plan to do the temperature calibration only occasionally and can easily wait for a little after issuing the command,

if I only knew after what time (1us? 1ms?) it is certainly finished.

Can you give some maximal duration?

Thanks, with best greetings

Gerhard